Reset Outgoing Call Quality Factor

Associated with: PSTN channels that are chosen due to their higher quality factor, rather than the fewest total calls

Security permission required to access this pick action: Diagnostics

Use this pick action to reset a PSTN channel’s Outgoing Call Quality Factor.

The pick action is only available if:

  • The method used for determining which channel is to call a PSTN outstation is set to Use channel with highest quality (see Define how a PSTN Channel is Selected for Communications in the Geo SCADA Expert Guide to Server Administration)
  • The channel’s Dial In/Out function is set to an option other than ‘Dial In Only’. (The option is specified on the Channel’s configuration Form.)