Software (XON/XOFF)

The Software (XON/XOFF) Flow Control setting manages the Flow Control software in the 'receiving' communications equipment. When Software (XON/XOFF) is selected the following steps occur:

The XON and XOFF signals are transmitted via the data connection between the 'sending' communications equipment and 'receiving' communications equipment.