Uncommanded Change Point

Associated with: Analog output points, digital output points and pulse controls for which a feedback point has been configured.

The attribute shows the name of the uncommanded change point associated with the point or pulse control.

For more information, see Configuring Control Checks Settings and see Uncommanded Change Settings.

Example:

Feedback.Uncommanded Input