Configuring Analog Points

Use EcoStruxure Web Services Analog Points to map analog ‘point’ data on EWS servers into Geo SCADA Expert in a format that it can understand, and vice versa.

Configure the properties of each Analog point using the fields on the EcoStruxure Web Services Analog Point Form.

This section covers configuration of the analog-specific properties on the EcoStruxure Web Services tab of the Form.

Use the EcoStruxure Web Services tab to:

For information on the Analog Point tab on the Analog Point Form, see Defining Analog Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the Control tab, see Define the Control Settings for an Analog Output Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the Control Checks tab, see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.