System Analysis

This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the Geo SCADA Expert system. This section applies specifically to the EtherNet/IP driver. For more general information on analyzing a Geo SCADA Expert system, see System Analysis.

During system analysis, you might need to:

Additionally, if a controller is not communicating with the server when it should be, see Troubleshooting.

When troubleshooting on a Geo SCADA Expert system, check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that Geo SCADA Expert has detected.