Specify the HCAL Store-and-Forward Cache Properties

Use the fields within the Store/Forward section of the AVEVA Historic Data Export tab to specify the properties of the HCAL store-and-forward cache. HCAL uses this cache to temporarily store export data if the network connection to the historian on the AVEVA application is unavailable or intermittent. Once the link becomes stable or available again, HCAL will forward the cached data to the historian.

Further Information

Specify a Folder for the HCAL Store-and-Forward Cache.

For further information about the historian on an AVEVA application, see the information about the historian in the documentation supplied with the relevant AVEVA application.