Alarm Limit Properties

Use the fields within the Alarm Limits section of the tab to define the limit properties of the point.

Use the High and High High fields to set the limits for the point, and to specify whether an event or alarm is generated if the point reaches these levels. For further information, see Configure the Limits for a Counter-Type Point in the Geo SCADA Expert Guide to Core Point Configuration.