Kingfisher Eavesdropping Arrangement

Eavesdropping allows a new system to run in parallel with an existing system in order to test the new system’ s configuration. The Kingfisher protocol uses an Rx eavesdropping arrangement.

Due to the flexible nature of the Kingfisher protocol, if you want to eavesdrop to a third-party server, we recommend that you contact Schneider Electric beforehand to confirm compatibility with Geo SCADA Expert.

For more information on eavesdropping, see Using Eavesdropping to Test a New Server’s Configuration.