Specify the Communications Re-Establishment Delay

Use the Delay while outstation performs a reset field to specify the delay between resetting a Kingfisher outstation and restarting communications.

The delay stops any messages from being sent to the outstation while it is in the process of resetting, then establishing communications with the server.