System Analysis

This section is designed for use by system administrators and high-level engineers when assessing the state of the Geo SCADA Expert system. It contains information that relates specifically to the Kingfisher Driver. For more general information on analyzing a Geo SCADA Expert system, see System Analysis in the Geo SCADA Expert Guide to the Server Status Tool.

During system analysis, you might need to:

Additionally, if an outstation is not communicating with the server when it should be, see Troubleshooting in the Geo SCADA Expert Guide to Advanced Drivers.

When troubleshooting on a Geo SCADA Expert system, examine the messages in the Events List. The messages may indicate the cause of any unexpected system behavior.