Display a Logic Program in Run Mode

When you display a Logic program in Run mode, you can view its operational status on the Geo SCADA Expert Server.

This allows you to:

To display a Logic program in Run mode:

  1. Log on to ViewX via a User Account that has the Operate feature enabled (on the User Form) and has the Read and Browse permissions for the Logic Program (or its parent Group).

  2. Display the Database Bar (see Display an Explorer Bar).
  3. Locate the entry in the Database Bar.
  4. Either:
    • Right-click on the entry and select Display <program type> from the menu that appears (where <program type> is the type of Logic program you have chosen to display).

    Or:

    • If your User account has the Double Click Edits Documents feature disabled, double-click on the program.

    The Logic program will display in Run mode.

Alternatively, you can display a Logic program in Run mode by performing one of the following:

  1. Display a Logic Program in Design Mode.
  2. Either:

    Or:

    • Deselect the Design Mode command on the ViewX ribbon's Edit tab.

    The Logic program will display in Run mode.

Or:

  1. Right-click on the Logic program in a Queries List.
  2. Select the Display option.

    The Logic program will display in Run mode.

Or:

  • Display the Logic program from a suitably configured Mimic.

Further Information

User Accounts and Security Permissions: see the Geo SCADA Expert Guide to Security.