Define the Severity of Lufkin SAMS Controller Events

Geo SCADA Expert assigns a severity level to the Lufkin SAMS controller events that it stores in the database. Use the Event Severity combo box on the Lufkin SAMS tab to specify the severity level that Geo SCADA Expert assigns to those events.


For more information about severity levels, see Defining Severities in the Geo SCADA Expert Guide to Core Configuration.

You use the Upload Event Log pick action to upload a controller’s events to Geo SCADA Expert (see Actions that are Specific to the Lufkin SAMS Driver).