Client Identifier

Associated with: MQTT Broker items

Geo SCADA Expert supports multiple connections to a broker, for which the combined Broker Host Address, Port, and Client Identifier settings have to be unique. This status attribute displays the broker's Client Identifier. This comprises the Client Identifier that is configured on the MQTT Broker's configuration Form.

 

The Client Identifier on an MQTT Broker has been configured as:

NorthRidge

This is the value that is shown for that Broker's Client Identifier status attribute.

Further Information

Client Identifier: see Configure the Broker Connection Properties.