Supported Communications Versions

The Sparkplug™ driver in Geo SCADA Expert is designed to enable Geo SCADA Expert to communicate with MQTT brokers in order to retrieve and/or control data on Sparkplug Edge Nodes and Sparkplug devices. In order to facilitate this:

  • The Edge Nodes have to be MQTT version 3.1.1 compliant client applications that manage the MQTT sessions.