ArcGIS Map Source
To configure a Map Source you use the Map Source tab of the Map Source Form (see Configuring a Map Source).
This topic describes the properties for an ArcGIS® Map Source.
ArcGIS is a geographic information system (GIS) for working with maps and geographic information. It is produced by the Environmental Systems Research Institute (ESRI), an international supplier of GIS software, web GIS and geodatabase management applications. ArcGIS map data is organized into layers, so that users can choose which layers they want to view or query. Geo SCADA Expert provides access to ArcGIS mapping as layers for Geo SCADA Expert composite maps. For more about map layers, see About Geo SCADA Expert Maps.
When you specify the Map Source as 'ArcGIS', the following properties are displayed on the Map Source tab:
- Map Source—Use this combo box to enter the type of this Map Source. In this case, you would select the ArcGIS option.
- Default Zoom—Define the default zoom level for this ArcGIS layer.
The Default Zoom level is the magnification level that Geo SCADA Expert will apply to a map layer when it first displays it. Users can then use manual controls to either zoom in or zoom out from this default level (that is, they can increase the magnification or decrease it). For more information, see Using a Geo SCADA Expert Map. If you increase the Default Zoom level, users will be able to see the map layer's features in greater detail. If you decrease the Default Zoom level, users will see less detail. The lowest zoom level is 0; this represents the lowest magnification level. The highest zoom level is 22; this represents the highest magnification level.
- Source URL—Enter the Uniform Resource Locator (URL) of the map on the ArcGIS server that you want to use for this layer. For example, an ArcGIS world map is at:
http://services.arcgisonline.com/ArcGIS/rest/services/World_Topo_Map/MapServer.For more information, see the ArcGIS services documentation.
-
Authentication URL—This property applies if the maps that you want to access are located on a federated server (that is, a server that has been integrated with the ArcGIS Enterprise portal). With such a server, authentication tokens are generated from a specific Authentication URL, instead of the map's Source URL. Use this field to enter the endpoint of the Authentication URL. If you are configuring an Authentication URL, you will also need to enter the Username and Password details for the tokens to be generated from the Authentication URL.
-
Username—If the maps that you want to access are from an authenticated source for which you have to specify security criteria, use this field to specify the username that provides access to those maps. ArcGIS authentication is performed via tokens that are fetched from the ArcGIS REST API. The account that you specify here is the one that is used to generate the ArcGIS tokens. The account has to have permission to generate the tokens.
Leave the field blank if you do not have to specify security criteria to access the maps.
-
Password—If the maps that you want to access are from an authenticated source for which you have to specify security criteria, use this field to specify the password that provides access to those maps.
Leave the field blank if you do not have to specify security criteria to access the maps.
- Layer Title—The Geo SCADA Expert title for this map layer. You can enter any title that you want. However, the title will appear on the Layer menu that Geo SCADA Expert map users can display, so aim to make the title as meaningful as possible (see Using a Geo SCADA Expert Map).
- Request Map as a Single Tile—Select this check box if you want the map to be displayed as a single tile at the requested magnification. This reduces the number of map requests that are sent to the service provider. Leave this check box clear if you want to use multiple tiles.
Requesting a map to display as a single tile reduces the number of requests to the server, however, this increases the bandwidth required. Using multiple tiles to display the map significantly increases the number of requests to the server, but will require less bandwidth.
- Overlay Layer—Select this box if you want this map layer to be an overlay. Clear this box if you want this map to be a base layer. For more information about overlays and base layers, see About Geo SCADA Expert Maps.
- Opacity—You can specify how transparent or opaque you want this map layer to be. This field will only be available if you select the Overlay Layer check box. The more transparent the layer, the more users will be able to see the graphical information in other map layers. You must enter a number between 0 and 1, where 1 is an opaque layer and 0 is a layer which is effectively invisible. For example, 0, 0.4, 0.7 and 1 are all valid entries. 1.5 is not a valid entry. If you set an Opacity of 0.1, Geo SCADA Expert will display a very faint rendering of the layer. As you increase the number towards 1, the more opaque the layer will be - and the layer will potentially become more likely to obscure the details of other layers. We recommend that you experiment with the Opacity setting to find the right balance.
- Refresh Frequency—Specify how frequently (in minutes) you want Geo SCADA Expert to send a request to the map server to update (refresh) the map layer data. This helps to ensure that a Geo SCADA Expert composite map shows the latest information for this layer. This field will only be available if you select the Overlay Layer check box.
- Display on Map Set by default—Select this check box if you want Geo SCADA Expert to display this map layer automatically when it loads a Map Set that includes this layer. Clear this check box if you do not want this map layer to display automatically. This field will only be available if you select the Overlay Layer check box.