Geographic Regions

A geographic region is an area that you can define on a map to enclose or group a set of related items. You can associate a region with a User, Users or User Group, which allows you to, for example, redirect alarms to the user responsible for a region (see Assign Regions of Responsibility).

There are three types of region items that you can create in Geo SCADA Expert:

Using these three types of region you can create:

  • multiple region items using any combination of the three types
  • overlapping regions
  • regions that exist within other regions.

You can include polygon regions on maps.

GeoJSON complexity can impact on server calculation time and client display time. We recommend that regions are as simple as possible to aid performance.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.