Add Text to a Mimic
You can add text boxes to your Mimics. The text boxes are rectangular and contain a string of characters that you define. You can set the text box to be transparent so that only the text is visible, or you can set it to have a color. Similarly, you can alter the appearance of the text. You can also animate text boxes (see Animations).
To add text to a Mimic:
- Select Text in the Drawing command group on the Graphics Tab.

When you position the cursor on the Mimic, it will appear as a cross hair. This indicates that the Text tool is selected.
- Draw a text box by pressing the left-hand mouse button and keeping it pressed down while you drag the cursor.
- Release the left-hand mouse button to complete the drawing of the text box and display the Text Properties window.
- Use the Text Properties window to define the settings for the text box.
Each tab provides the following settings:
- General—Use to access the Animations and Pick Action settings, define the ToolTip, enable or disable Visibility, and define Dynamic Positions.
- Text—Use to define the text that is shown in the text box.
- Pen—Use to define the color and shading settings of the text.
- Fill—Use to define the color and shading settings of the text box.
- Font—Use to define the style and size of the text.
You can find more detailed information about the Text properties window in Editing a Text Box.
- Close the Text Properties window.
You can reposition the text box by dragging it, or you can double-click on it to edit it (see Editing a Text Box).
You can also access editing features by right-clicking on the text box to display a context sensitive menu (see Mimic Editing Features).
Further Information