Adding Objects to a Mimic
You can add a variety of objects to your Mimics, including shapes, comments, and dynamic values (referred to as animations). In this section, we explain the various ways in which you can add or insert mimics.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
For information on adding dynamic values (values that update according to the values that are stored in the database), please refer to the Animations section (see Animations).
You can also add imported images to a Mimic. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Further Information