Displaying a Mimic

There are various techniques you can use to display a Mimic, some of which are only available if your User account is configured to have certain features enabled or has specific security permissions. In the following sections, we describe the various ways in which you can display a Mimic, explain the difference between the two Mimic modes (Run Mode and Design Mode), and also provide an overview of the Mimic interface.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.