Display the Layers Window

To add, remove, or reorder the layers for a Mimic, you need to access the Layers window.

To access the Layers window:

  1. Display the Mimic that you want to edit in Design mode.
  2. On the Graphics Tab, select the Layers command from the View command group.

    The Layers window is displayed.

The Layers window contains a list of the layers that are already set up for the Mimic (if any). Information about the layers is shown in the following categories:

The Layers window also contains the following buttons:

Do not confuse Mimic Layers with Mimic Views. To specify the level of magnification at which a Mimic is displayed when it is opened in Run mode, see Setting a View as the Default View.

Further Information

Switching Between Layers on a Mimic in Run mode.