Editing an Embedded Query List

When you have added an embedded list to a Mimic, you can access its Embedded List Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Embedded List Properties window contains four tabs. For more information concerning each tab, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.