FlashGradAlpha

The FlashGradAlpha property defines the amount of transparency that is applied to the FlashGradColour. This works in the same way as the FillAlpha property except that it applies to the second alternate color used with 3 color flash effects.