FlashOffset

The FlashOffset works in exactly the same way as the FlashOffset property in the Fill group except that it applies to the flash sequence for the line/outline rather than the fill. Typically, you would set the flash offset on the Polyline Properties window (it is not designed to be used as an animation).