Flipping a Mimic Object

You can flip a Mimic object so that it appears as a mirror image of its original shape. This is useful for converting left-facing objects into right-facing objects and vise-versa. For example, you can use the flip tool to change corner pieces like this:

The Flip feature is only available for Pipes, Lines, and Shapes.

To flip an object:

  1. Display the relevant Mimic in Design mode.
  2. Right-click on the Mimic object that you want to flip.
    A context sensitive menu is displayed.
  3. Select the Flip option, then choose from:
    • Horizontal—Flips the object from left to right or vise-versa.
    • Vertical—Flips the object from top to bottom or vise-versa.

You can also access the Flip options via the Orientation command in the Arrange group on theGraphics Tab.