Modbus Function Codes Supported by the Geo SCADA Expert Simple Modbus Driver

The Geo SCADA Expert Simple Modbus Driver supports several Modbus function codes, enabling it to read and write data on Modbus devices. The function codes that the Geo SCADA Expert Simple Modbus driver supports are:

Modbus Function Code Functionality

FC1

Read output coils

FC2

Read input discretes

FC3

Read multiple holding registers

FC4

Read input registers

FC5

Write coil

FC6

Write single register

FC15

Write multiple coils

FC16

Write multiple registers

FC65

Read S600 flow computer single-precision registers

FC67

Read S600 flow computer double-precision registers

An exception error is generated if an unsupported function code is received by a Modbus device (see Modbus Exception Errors).