Modbus Function Codes Supported by the Geo SCADA Expert Modbus Slave Driver

The Geo SCADA Expert Modbus Slave Driver supports several Modbus function codes, enabling it to read and write data using the Modbus protocol. The function codes that the Geo SCADA Expert Modbus Slave driver supports are:

Modbus Function Code Functionality

FC1

Read output coils

FC2

Read input discretes

FC3

Read multiple holding registers

FC4

Read input registers

FC5

Write coil

FC6

Write single register

FC15

Write multiple coils

FC16

Write multiple registers