Specify the Value Maps that Store the Source Data

Modbus Slaves use Value Maps to store ‘point’ data. Each Source within a Slave can store data using a different set of Value Maps.

The Value Maps that are required for the Slave need to have been created and suitably configured on your system (see Using Value Maps to Represent Modbus Data Address Ranges in this guide, and see Configuring Value Maps in the Geo SCADA Expert Guide to Core Configuration).

Use these Map fields on the Source tab to define the Value Maps that are used by a particular Source:

Leave the fields blank for any Map types that are not used by this Source.

Each field and associated Value Map represents a different type of data within a Modbus PLC. For example, if a Value Map is specified in the Input Register Map field, above, the entries that populate the Value Map would emulate Input Register data in a Modbus PLC. For more information, see Using Value Maps to Represent Modbus Data Address Ranges.

For an example of how you might use a Value Map to represent Modbus data and how you might map that data to a Modbus Slave Source, see Example Configuration.