Understanding NTP Stratum Ranking and how this Affects Clock Accuracy

The NTP protocol uses strata to indicate the expected accuracy of system clocks. The device that has the most accuracy is the ‘reference’ clock—the clock with which the other devices on the system, such as workstations and servers, synchronize their time.

A machine’s time can be synchronized directly with the ‘reference’ clock, or via another machine (an ‘NTP Server’) which either synchronizes its own clock directly with the ‘reference’ clock, or with the clock of another NTP server. Each level of synchronization is assigned a different stratum number. The lower the stratum number or level, the higher the accuracy of the system clock(s) at that level. Additionally, each clock’s accuracy is also affected by the stability of the ‘reference’ clock itself, and the particular network path(s) that are used for the NTP time synchronization.

In summary:

The furthest possible level is Stratum 16. A machine at this level is deemed to not have a synchronized time source.

A machine that has just started up will initially be at Stratum 16, until it synchronizes its clock with an NTP server (or directly with the ‘reference’ clock). Once synchronized, its stratum will update to indicate its new level. (Should synchronization be unsuccessful, the machine will remain at Stratum 16.)

With machines that are configured to synchronize their system clocks via one of several NTP time sources, the stratum level can vary, depending which source is used. Such machines synchronize with whichever NTP time source has the lower Stratum level (and therefore the highest time accuracy). If both time sources are at the same Stratum level, the machine will synchronize its clock with whichever NTP device it is able to communicate with first.

Be aware that whenever a machine synchronizes its time and that synchronization causes its clock to update its time by a significant amount, that machine will indicate Stratum 16 and attempt to further re-synchronize its time. On Geo SCADA Expert systems on which the NTP Monitor driver is being used to monitor a machine’s stratum and a stratum of 16 is configured to raise an alarm, such a situation will result in ‘false positives’—an alarm will be raised due to the machine synchronizing its clock successfully if, in doing so, that synchronization causes the clock’s time to change significantly.

You can achieve high accuracy time (such as synchronizing time to within an accuracy of 1ms) using W32Time, providing that certain criteria are satisfied. For more information, see https://learn.microsoft.com/en-us/windows-server/networking/windows-time-service/support-boundary. However, if you choose to use another third-party NTP client to maintain accurate time, remember to disable Windows Time (W32Time).