Configure SQL Query Lookup Properties

Use these fields on the ODBC tab to specify general and SQL Query Lookup properties of a point. The fields at the top of the tab are common to points on many simple drivers (see Configure Common Point Properties in the Geo SCADA Expert Guide to Simple Drivers).

Fields that are specific to the ODBC driver are explained below: