Configure General Properties on the OPC Tab

Use the fields at the top of the OPC tab to configure the general point properties of each point. Some of these fields are common to many simple drivers (see Configure Common Point Properties in the Geo SCADA Expert Guide to Simple Drivers). Fields that are specific to points on the Simple OPC driver are explained below.