Enable Subscription

Associated with: OPC UA Subscription items

Security permission required to access this pick action: Disable Points

Use this pick action to place an OPC UA Subscription database item In Service. Triggering the action changes the Subscription's configuration so that its In Service property is enabled and the Subscription becomes active.

The Enable Subscription pick action is only available for an OPC UA Subscription:

  • That is not In Service
  • For which your User Account is allocated the Disable Points security permission.
NOTICE

unexpected impact on system performance

It is possible that excessive incoming data from an OPC UA server could adversely affect system performance. If performance is an issue, check:
Failure to follow these instructions can impact adversely on system performance.

Also see Disable Subscription.

If using this pick action with the Automation Interface, you need to specify the method name Enable.