Configure the Common Pager Service Properties

The Pager Service configuration Form contains several tabs. The Identification, User Methods, Alarm, and Redirection tabs are common to many types of database item (see Tabs on Configuration Forms). The <Pager> Service tab is specific to Pager Services and varies according to the type of Pager Service. For example, the Form for a TAP Pager Service has a TAP Service tab.

Each <Pager> Service tab contains properties that define how Geo SCADA Expert uses the Pager Service. Some of these properties are available for multiple types of Pager Service (common properties), while others are specific to a certain type. For example, the Multitone Pager Service Form and the UCP Pager Service Form both have the 'common' Maximum Message Length property, but only the UCP Pager Service Form has the Standard Reply Delay property (this is a UCP-specific property).

In this section, we explain how to use those properties that are available on the <Pager> Service tab of the Pager Form for multiple types of Pager Service (these are the 'common' Pager Service properties):

For information on those properties that are specific to a particular type of Pager Service, you should refer to the relevant section:

Multitone Pager Services only have common configuration properties (they have no service-specific configuration properties).