Access the Documentation about the Python Client Library

In order for your Python programs to interact with the Geo SCADA Expert database, you have to refer in your program code to the relevant classes and functions that are in the Python client library for Geo SCADA Expert. The documentation about these classes and functions is installed when you install the Python driver components on the Geo SCADA Expert server, or the Data Access component on a client machine.

To access the separate ‘Python client library for Geo SCADA Expert’ documentation suite:

  1. In Windows, select the Start menu.

  2. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder.

  3. Select the entry for the Python Client Library Guide.