Define the Location of the Python Executable
The Python section of the Server Configuration Tool includes an Executable field.
In order for the Geo SCADA Expert server to be capable of executing Python programs, in addition to installing the Python driver on the server, you also need to install the Python executable and Python Package files (see Install the Required Python Components on the Server).
Use the Executable field to specify the location of the Python .exe (executable) file on the Geo SCADA Expert server. Use the Browse Button to display a window. Locate and select the Python executable file from the window. Ensure that you select the relevant executable file - you might find that other applications on the server also use Python functionality via other Python executable files.