StdErr Timestamp

Associated with: Python Program items

This status attribute indicates the date and time at which the latest run of the Python program generated standard error (StdErr) content.

Use in conjunction with the StdErr status attribute. Both status attributes are only included in the Status display if the latest run of the Python program resulted in standard error content being generated.