StdOut Timestamp
Associated with: Python Program items
This status attribute indicates the date and time at which the latest run of the Python program generated standard output (StdOut) content.
Use in conjunction with the StdOut status attribute. Both status attributes are only included in the Status display if the latest run of the Python program generated standard output content.