Specify the Geo SCADA Expert Port for the GSM Modem

Use the Port field on the Connection tab to specify the Geo SCADA Expert COM port to which the Geo SCADA Expert GSM modem is connected (see Configure a Channel's Serial Connection Properties in the Geo SCADA Expert Guide to Drivers).