Define the Delay While a Controller Performs a Reset

Use the Delay while outstation performs a reset field in the SCADAPack Modbus section of the tool to specify the delay between resetting a controller and restarting communications. The delay helps to prevent any messages from being sent to the controller while it is in the process of resetting and then establishing communications with the server.