Using SCADAPack Modbus Specific Actions
Geo SCADA Expert supports a wide variety of operator-driven or automated actions and controls. When performed by an operator,
Most pick actions exist as 'methods' (specifically 'action methods') in the database. The pick actions that are available in ViewX and Virtual ViewX represent just some of the methods that are available in Geo SCADA Expert. (Methods that are designed only to be used programmatically are not made available as pick actions.)
Users with the required permissions can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions). See a system administrator for the documentation associated with such custom actions (also known as 'methods').
The SCADAPack Modbus driver supports a combination of:
- Actions that are common to many database items (see Object Menu, and see Object Menu Options)
- Actions that are common to database items on many drivers (see Actions that are Common to Many Drivers)
- Actions that are driver-specific. The topics in this section provide information about the actions that are specific to database items on this particular driver. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
NOTE: This section is about pick actions that are specific to this driver. In addition to the pick actions mentioned here, this driver's extension drivers might support further pick actions. For information about driver-specific pick actions that are not covered in this section, see the relevant extension driver guide.