Configure Modbus Server Device Configuration Settings

The Configuration section of the Modbus tab allows you to specify the settings that enable the SCADAPack x70 to scan the Modbus Server device.

Register Addressing

Use this combo box to specify whether the register addresses that the SCADAPack x70 uses to communicate with the Modbus Server have 5 digits or 6 digits. Be aware that each type of device has its own specific address range—refer to the device documentation for the address range that applies to a specific type of device.

Select the addressing mode that matches the mode used by the Modbus Server.

Modbus Data Type SCADAPack x70 Configuration Type 5-Digit Address Range 6-Digit Address Range

Coil,
Discrete Output

Digital Output Point, Digital Input Point

1 to 9999

1 to 65535

Discrete Input

Digital Input Point

10001 to 19999

100001 to 165535

Input Register

Analog Input Point, Digital Input Point, Counter Input Point

30001 to 39999

300001 to 365535

Holding Register

Analog Output Point, Digital Output Point, Analog Input Point, Digital Input Point, Counter Input Point

40001 to 49999

400001 to 465535

Default Scan Rate

The time interval at which the SCADAPack x70 executes the configured scans. Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value. The valid range is between 10 ms and 999999999 ms inclusive. The default value is 500 ms (0.5 seconds).

If the Maximum Consecutive Timeouts is exceeded, and the Default Scan Rate is set faster than 15000 ms (15 seconds), the scan rate is automatically slowed to 15 seconds to accommodate the ongoing communications interruptions.

The scan rate returns to the configured Default Scan Rate after the first successful scan and response.

Maximum Consecutive Timeouts

Enter the number of times that the SCADAPack x70 should attempt to send a message to the Modbus Server before it determines that it cannot communicate with the device.

If the Maximum Consecutive Timeouts is exceeded, and the Default Scan Rate is set faster than 15000 ms (15 seconds), the scan rate is automatically slowed to 15 seconds to accommodate the ongoing communications interruptions.

Timeout

The amount of time the SCADAPack x70 waits for a reply to a read or write command before considering communications with the device to be interrupted. Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value. The valid range is between 0 ms and 65530 ms inclusive. The default value is 1000 ms (1 second).

Write Coils

Use this combo box to select the function code that is supported by the Modbus Server to be scanned. Select from the following:

Multiple (Function Code 15)

This allows multiple coils to be set on or off in a single message. If supported by the Modbus Server this allow for more efficient communications.

Single (Function Code 5)

This allows a single coil to be set on or off in a single command. This is less efficient when controlling a block of consecutive coils.

Write Holding Registers

Use this combo box to select the function codes that are supported by the Modbus Server to write data to holding registers. Select from the following:

Multiple (Function Code 16)

Used to write data (2 bytes per register) to a block of contiguous holding registers (1 to 123 registers). If supported by the Modbus Server this allow for more efficient communications.

Single (Function Code 6)

Used to write data (2 bytes) to a single holding register. This is less efficient when controlling a block of consecutive registers.

This option impacts on the type of analog data to which the Server Device's Modbus Point Scanners can write. The option restricts the number of Modbus Data Type options that are available to a Modbus Point Scanner when that Scanner's Operation is set to 'Write' or 'Read/Write' (see Configure the Modbus Scanners Settings).

Modbus Byte Order

The order of the bytes sent to a Modbus Server. Select the byte order and word order combination that matches the order used on the Modbus Server.

The order you select is used for 32-bit and 16-bit register values, but the second part of the selection — the word order — is not used for 16-bit values because these values consist of just 2 bytes, or 1 word.

  • For 32-bit register values, 2 bytes (1 word) are contained in the first register, and 2 bytes (1 word) are contained in the second register.
  • For 16-bit register values, the 2 bytes (1 word) are contained in the only register. A second register is not required.

In the setting description, the numbers 1 (Most significant), 2, 3 and 4 (Least significant) represent the 4 bytes in a 32-bit register value and 1 is the most significant byte.

High Byte/Low Word First (3412)

Sends 32-bit values in byte order 3412

Sends16-bit values in byte order 12

High Byte/High Word First (1234)

Sends 32-bit values in byte order 1234

Sends16-bit values in byte order 12

Low Byte/High Word First (2143)

Sends 32-bit values in byte order 2143

Sends16-bit values in byte order 21

Low Byte/Low Word First (4321)

Sends 32-bit values in byte order 4321

Sends 16-bit values in byte order 21

When the Realflo Flow Computer option is selected in the Device Configuration Options section of the Settings tab and the IP Address in the Communication section is set to '127.0.0.1' , the Modbus Byte Order is fixed at 'High Byte/High Word First (1234)'.

Modbus Bit Order

This section allows you to define the bit order for register data sent to a Modbus Server. The bit order selection is applied to every byte that is sent regardless of the byte order. The default settings should only be changed if required.

Select the bit order that matches the order used on the Modbus Server.

Most significant bit first

Sends the most significant bit first.

Least significant bit first

Sends the least significant bit first.