Configure the Connection to the Controlling Station

Use the fields within the Connection to Controlling Station section of the DNP3 Outstation tab to specify how many controlling stations will communicate with the outstation and configure the settings that apply when the SCADAPack x70 device attempts to send an unsolicited event message to a controlling station.

Number of Controlling Stations

Use this combo box to select the number of controlling stations with which the outstation is to communicate. The maximum available is three. One of the controlling stations should be this Geo SCADA Expert system. Other controlling station(s) might comprise other Geo SCADA Expert system(s) or third-party DNP3 controlling station(s). Any of the controlling station can be the 'local' controlling station—the controlling station that is being used to configure the outstation.

If you are connecting to more than one controlling station the fields associated with those controlling station(s) become active.

If the outstation is configured to communicate with multiple controlling stations, other field(s) become available on the configuration Forms of the points on this device.

DNP3 Outstation Address

Use to specify the address of the outstation as used by the controlling station when communicating with this outstation. Values can be 0 to 65519, default is 0.

DNP3 Controlling Station Address

Use to specify the address of the Controlling Station with which the outstation communicates. Values can be 0 to 65519, default is 30000.

Unsolicited Allowed

Select the check box if the outstation is to send event data to the DNP3 controlling station using unsolicited messages. Other fields within this section of the tab become available for use. When this check box is selected, the DNP3 Routing table has to have a corresponding route that includes the DNP3 Outstation Address in the Source address range and the DNP3 Controlling Station Address in the Destination address range (see Add and Configure the Entries in a DNP3 Routing Table).

Ensure that the check box is clear if the outstation is to send event data to the DNP3 controlling station only in response to requests from that DNP3 controlling station. This is the default setting.

Communications Port

Use this combo box to specify the port via which the outstation is to send unsolicited messages to the DNP3 controlling station. You can only specify a port that has its Function set to DNP3 or PPP/TCPIP(see Device Configuration Serial Port Tabs). If you specify an Ethernet port, you also have to Set up the Ethernet Link Layer. The number of serial and Ethernet ports depends on the SCADAPack model.

Minimum Unsolicited Event Tx Delay

Specify the minimum time between consecutive unsolicited messages sent by the outstation. This field is available if unsolicited messages are allowed. The default setting is 30 seconds.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Quiet Time Delay

Specify the amount of time that the outstation is to wait if it has tried to send an unsolicited message for the maximum number of Unsolicited Attempts Per Burst and has still not received a response from the DNP3 controlling station (see Unsolicited Configuration).

Once the Quiet Time Delay has elapsed, the outstation will attempt to resend the unsolicited message for up to the maximum number of Unsolicited Attempts per Burst again. This cycle is repeated until it receives a response from the DNP3 controlling station. The default is 2 minutes.

Application Layer Confirm (Event) Timeout

Specify the maximum amount of time that the outstation waits for:

  • Confirmation of an unsolicited response sent to the DNP3 controlling station.
  • Confirmation of a poll response that contains event data.

When the outstation receives the confirmation, the events that were sent in the response are deleted from the outstation’s internal Event Buffer.

The default is 16 seconds. Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.