Display Modbus Point Scanners

Associated with: SCADAPack x70 Device Configuration items and SCADAPack x70 Modbus Server Devices

Security permission required to access this pick action: Read

This topic only applies to systems on which SCADAPack x70 Modbus Point Scanners have been created manually. When your Modbus Server Devices are configured to automatically create their scanners then the database will not contain any Modbus Point Scanners (see Configure Modbus Point Scanners Settings).

Use the Display Modbus Point Scanners pick action to display a Queries List of SCADAPack x70 Modbus Point Scanners that are associated with the selected SCADAPack x70 Device Configuration item or SCADAPack x70 Modbus Server Device.

This pick action is not a method and therefore cannot be used with the automation interface.