Downloaded Security File

Associated with: SCADAPack x70 DNP3 Outstations that use DNP3 secure authentication.

This status attribute indicates:

  • The name of the last .rtk file to be downloaded to the SCADAPack x70 device with which the SCADAPack x70 Outstation item is associated
  • A time stamp showing the last modification date and time of the file.

    Example:

    "system.rtk" Modified at 27/04/2010 09:33:37.000

This status attribute is only displayed if the Download Security Configuration pick action has been used to successfully download a security configuration file to the SCADAPack x70 device. (The security configuration file is an .rtk file that has been imported into Geo SCADA Expert using a SCADAPack x70 Security Configuration database item.)

Use this status attribute in conjunction with the Downloaded Security Description status attribute to ascertain information about the .rtk file that was last downloaded to the SCADAPack x70 device.

For more information, see Import Security Configuration.