Import/Upload Status

Associated with: SCADAPack x70 Device Configuration items.

The Import/Upload Status status attribute indicates the phase of an import/upload transaction, and the percentage of progress of an ongoing import/upload transaction.

When the import/upload transaction is queued, the status attribute displays the following information:

Transaction: Queued: Progress:<percentage>% completed

When the import/upload is in progress, the information that is displayed differs depending on the phase, but will comprise one of the following:

Transaction: Updating: Progress:<percentage>% completed

Transaction: Deleting: Progress:<percentage>% completed

Transaction: Finalizing: Progress:<percentage>% completed

When the import/upload is completed, this status attribute displays the following value:

Transaction: Idle

The 'idle' status of the transaction indicates the last transaction to have been attempted/completed.

 

The following examples show the type of information that is displayed at each phase:

When the import/upload transaction is queued, the status attribute displays the following type of information:

Transaction: Queued: Progress: 00.00% completed

When the import/upload is in progress, the status attribute displays information about the current phase of the import/upload.

The first phase comprises updating the database:

Transaction: Updating: Progress: 20.45% completed

The second phase comprises marking any obsolete database items for possible deletion:

Transaction: Deleting: Progress: 60.30% completed

The third phase comprises finalizing the import/upload:

Transaction: Finalizing: Progress: 98.25% completed

Use this status attribute alongside the Import/Upload Summary status attribute to monitor the progress of an import/upload transaction.