Security File
Associated with: SCADAPack x70 Security Configuration items.
This status attribute indicates:
- The name of the last .rtk file to be imported into the Security Configuration item.
- A time stamp showing the last modification date and time of the file.
Example:
"system.rtk" Modified at 2025-05-29 10:05:32
This status attribute is only displayed if the Import Security Configuration pick action has been used to successfully import a security configuration file from the Security Administrator software.
Use this status attribute in conjunction with the Security Description status attribute to ascertain information about the .rtk file that was last imported into the Security Configuration item.
For more information, see Import Security Configuration.