Confirm that the SE RPC Server Component is Installed

The SE Rod Pump Controller extension driver provides the Advanced Modbus driver with extra functionality, enabling Geo SCADA Expert to monitor rod pump activity via Schneider Electric Rod Pump Controllers. In order to monitor such data, the Schneider Electric Rod Pump Controller component has to be installed on each of the servers on your system (including any permanent standby servers), in addition to the Advanced Modbus component.

Use the Add/Remove Programs function in the Windows® Control Panel to check whether the required components are installed.

The Schneider Electric Rod Pump Controller component is located in the Server group, in a branch off from its Advanced Modbus ‘parent’ driver component. To check that this component has been installed, ensure that the symbol to the left of the text Schneider Electric Rod Pump Controller does not have an X on it.