Driver Logging Options that are Specific to the SE RPC Driver

This section is for system administrators and high-level engineers who need to use diagnostic information to assess the state of the Geo SCADA Expert system. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the logging options that are supported by this extension driver.

As an extension driver, this driver supports the logging options of its 'parent' driver in addition to its own driver-specific logging options.

You access both sets of logging options using the Logging window of the parent driver. The Logging window contains both the parent driver's logging options and those of whichever extension drivers are installed. As with any driver, you view the logging options using the Modules section of the Geo SCADA Expert Server Status Tool (see Define the Driver Logging Settings).

These driver logging options are specific to this extension driver:

  • POC Card Retrieval—Logs information relating to the retrieval of current dynacard data.
  • POC Historic Retrieval—Logs information relating to the retrieval of historic point data.

 

Further Information

Logging options supported by this driver's parent driver: see Driver Logging Options that are Specific to the Advanced Modbus Driver.

Common Advanced Driver Log File Options.