CaseExpression

Functions selecting a value conditionally

Contents

Name Description
Case abbreviation COALESCE Returns the first operand that is not equal to NULL. If all operands are NULL then returns NULL
Case abbreviation NULLIF Returns NULL if the operands are equal otherwise returns the first operand
Searched case Selects one from a number of alternate values
Simple case Selects one from a number of alternate values