Conditions.bool-primary-unique

Returns True if all rows in the result set are unique (distinct)

Format

UNIQUE ( query-expr )

Remarks

Used to test if every row in a result set is unique i.e. there are no duplicates.

Example:

SELECT A.NAME FROM A WHERE NOT UNIQUE ( SELECT B.DESC FROM B WHERE B.ID = A.ID )