Conditions.bool-term

Returns True if all of the bool-factors are True

Format

bool-factor [ AND bool-factor ] *

Remarks

A bool-term consists of one or more bool-factor separated by AND operators.

The result of a bool-term is False if any of the bool-factor are False, otherwise.

The result of a bool-term is Unknown any of the bool-factor are Unknown, otherwise.

The result of a bool-term is True only if all of the bool-factor are True.

The AND operator is higher precedence than the OR operator.